Observing an event via the "UaExpert" OPC UA Client Permalink

  1. Start the ‎UaExpert‎ program.

  2. Click “Server  Add”.

    The “Add Server” dialog opens.

  3. In the tree view, expand “Local  OPCUAServer@”.

  4. Select the connection type “None” and click “OK” to close the dialog.

  5. Click “Server  Connect”.

    An object tree is displayed in the “Address Space” view.

  6. Click “Documents  Add”.

    The “Add Document” dialog opens.

  7. Select the “Event View” as the "Document Type".

    The “Event View” tab opens.

  8. In the “Address Space” view, expand the “Objects  DeviceSet CODESYS CODESYS Control Win V3” object.

  9. In “Address Space”, select the "CODESYS Control Win V3" object and drag it to the “Event View”.

    The events are displayed.

    _cds_img_uaexpert_3.png